MCIMX6Y2CVM05AB upgrade to MCIMX6Y2CVM08AB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCIMX6Y2CVM05AB upgrade to MCIMX6Y2CVM08AB

481 次查看
michael_yang
Contributor II

for CPU upgrade, what changes are needed to the software?

0 项奖励
回复
2 回复数

424 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @michael_yang,

I hope you are doing well
 
Both part number has the below differences.
MCIMX6Y2CVM05AB: 528 MHz, industrial grade for general purpose
MCIMX6Y2CVM08AB: 792 MHz, industrial grade for general purpose
 
According to the values written in the SPEED_GRADING[1:0] fuses, the frequency will be selected from the U-boot as mentioned in soc.c file.
 
Hence No software changes are required.
 
The fuse SPEED_GRADING[1:0] can be referred from the Table 5-9. Fusemap Descriptions from the reference manual IMX6ULLRM.
 
Thanks & Regards,
Dhruvit Vasavada
0 项奖励
回复

173 次查看
michael_yang
Contributor II

@Dhruvit 

For MCIMX6Y2CVM08AB, How to set SPEED_GRADING[1:0] to 800M? PROD/SW I don't know how to process it.

michael_yang_0-1720689445033.png

 

0 项奖励
回复