iMXRT - supporting GUI libraries.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMXRT - supporting GUI libraries.

ソリューションへジャンプ
6,128件の閲覧回数
johnot
Contributor I

Hi,

  I have the following queries for  iMXRT

  1.         Do the iMXRT BSP contains any free graphic library?.
  2.         Is there any third party free graphic library tested with iMXRT by any customer?
  3.         iMXRT supports ucLInux.  What is the foot print of it? What is the linux kernel version?  What graphic library tested with UCLINUX?
  4.       Is emwin graphic library available with iMXRT?

Best regards,

John OT

0 件の賞賛
返信
1 解決策
5,142件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi John OT,

About your above questions, replies are as follows:

1\Yes, the emwin graphic library available.

2\ Do not known by now

3\ The ucLInux is the third party company supply, you can refer to :

Linux BSP for the NXP i.MX RT1050 EVK Board 

4\Yes

Have a nice day

Rita

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
5,142件の閲覧回数
johnot
Contributor I

Hi Rita,

  Thanks for your reply.  I just want to know one more thing. Is the emwin graphic library with iMXRT freely available?

Is it possible to use emwin graphic library in imxrt based commercial productes free of cost?

Best regards,

John OT

0 件の賞賛
返信
5,142件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi John OT,

Yes, the emwin graphic library with iMXRT  is freely available. You can use it.

Have a great day,
Rita

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
5,142件の閲覧回数
anjalikkrishna
Contributor III

Hi Rita,

   I am using SDK 2.4.0 for i.MXRT EVKB board and the boot device is QSPI. I am able to flash and run non-XIP programs to QSPI like hello world. But could not succesfully  flash xip emWin application 

The SDK  does not allow to uncheck xip driver when emWin is selected.

According to this How to i.MXRT1051 QSPI Boot w/o XIP (Reside in Flash, Run from TCM)  QSPI does not support xip in i.MXRT1051 .

Whether QSPI supports xip in i.MXRT1050 EVKB BOARD?

 Whether the emWin applications be built without xip driver included.?

Regards,

Anjali

0 件の賞賛
返信
5,142件の閲覧回数
johnot
Contributor I

Hi Rita,

 

   Thanks for the quick reply.

 

  Have couple of questions.

  1. We didn't want to use hyper flash, instead we want to use either QSPI or SD card.

  2. Can we use sd card to boot the system and run the emwin gui? Is tools are available to program the SD card from out side and use it in RT board? 

  3. Can we use qspi with emwin gui? Since emwin occupy a bigger amount of memory, is it wise to use QSPI for booting? Is tools are available to program the qspi  with USB/uart  connections with PC?

 

Best regards,

John OT

0 件の賞賛
返信
5,142件の閲覧回数
johnot
Contributor I

Hi Rita,

   Thanks for the quick reply.

  Have couple of questions.

  1. We didn't want to use hyper flash, instead we want to use either QSPI or SD card.

  2. Can we use sd card to boot the system and run the emwin gui? Is tools are available to program the SD card from out side and use it in RT board? 

  3. Can we use qspi with emwin gui? Since emwin occupy a bigger amount of memory, is it wise to use QSPI for booting? Is tools are available to program the qspi  with USB/uart  connections with PC?

Best regards,

John OT

0 件の賞賛
返信
5,143件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi John OT,

About your above questions, replies are as follows:

1\Yes, the emwin graphic library available.

2\ Do not known by now

3\ The ucLInux is the third party company supply, you can refer to :

Linux BSP for the NXP i.MX RT1050 EVK Board 

4\Yes

Have a nice day

Rita

0 件の賞賛
返信