iMX95: Compilation error with bitbake.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX95: Compilation error with bitbake.

990 Views
danielsan-77
Contributor I

I want to compile from the source code, but I get errors when compiling it for the iMx95. I am working with a computer with Ubuntu 18.04. To do this I follow the steps of I have followed the steps of https://dev.variscite.com/dart-mx95/mx95-yocto-walnascar-6.12.49_2.2.0-v1.0/yocto-build-release/

Specifically, when launching the "bitbake fsl-image-gui-chromium" I get this error:

ERROR: OE-core's config sanity checker detected a potential misconfiguration.
Either fix the cause of this error or at your own risk disable the checker (see sanity.conf).
Following is the list of potential problems / advisories:

Fetcher failure for URL: 'https://www.yoctoproject.org/connectivity.html'. URL doesn't work.
Please ensure your host's network is configured correctly.
Please ensure CONNECTIVITY_CHECK_URIS is correct and specified URIs are available.
If your ISP or network is blocking the above URL,
try with another domain name, for example by setting:
CONNECTIVITY_CHECK_URIS = "https://www.example.com/" You could also set BB_NO_NETWORK = "1" to disable network
access if all required sources are on local disk.
Summary: There was 1 ERROR message, returning a non-zero exit code.

I have also tried other previous versions, but the same thing happens.

The same error occurs if I launch other bitbakes.

All the best,
Daniel.

 

0 Kudos
Reply
2 Replies

966 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

I suggest you check directly with Variscite since our BSP is built and requirements are different.

Please check if this is a known issue in the recipe or if you have some kind of firewall issue since you have fetch errors.

Best regards.

0 Kudos
Reply

946 Views
danielsan-77
Contributor I

Thank you!

0 Kudos
Reply