iMX8X - how to build SCFW to match official NXP SCFW binary file ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8X - how to build SCFW to match official NXP SCFW binary file ?

1,236 Views
LaurentBardet
Contributor III

Dear support,

Could you clarify which compilation options are required to generate SCFW (as describer in imx_scfw_porting_kit_1.2.2), to match scfw-tcm.bin as fetched from NXP during Yocto build ?

Currently we face different behaviour during linux start on IMX8QXPMEK board:

A/ With default scfw-tcm.bin file (as fetched June 11th through YOCTO):

linux boot success (tycally can run graphic demos).

B/ with regenerated scfw-bin from imx_scfw_porting_kit_1.2.2 package:

linux boot failed during starup, complaining about access to graphic resources

I can provide you with detailed serial traces on both UART0 and M4 UART.

best regards,

Laurent

0 Kudos
Reply
1 Reply

988 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Laurent,

I’m afraid that i.MX8QXP is still on preproduction and no additional information/support could be provided yet. For further assistance, please contact with your NXP FAE/Sales or with your DBM.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 Kudos
Reply