iMX8QXP: Support multiple RAM sizes with same scfw/u-boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8QXP: Support multiple RAM sizes with same scfw/u-boot

ソリューションへジャンプ
1,834件の閲覧回数
mod42
Contributor III

Is it possible to populate an iMX8QXP based board with different RAM sizes (8Gb, 16Gb, 24Gb, 32Gb) and handle this with the same scfw/u-boot/kernel image? Different RAM sizes would be configured in user fuses. scfw should then dynamically adjust the RAM size according to the fuse settings. Is there an example for such an approach?

0 件の賞賛
返信
1 解決策
1,790件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

No this is not possible, please note that ROM code will read and execute the SCFW, this will include the DDR initialization. Also, we do not have such approach.

Best regards,
Aldo.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,791件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

No this is not possible, please note that ROM code will read and execute the SCFW, this will include the DDR initialization. Also, we do not have such approach.

Best regards,
Aldo.

0 件の賞賛
返信