iMX8QXP: Support multiple RAM sizes with same scfw/u-boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8QXP: Support multiple RAM sizes with same scfw/u-boot

Jump to solution
1,882 Views
mod42
Contributor III

Is it possible to populate an iMX8QXP based board with different RAM sizes (8Gb, 16Gb, 24Gb, 32Gb) and handle this with the same scfw/u-boot/kernel image? Different RAM sizes would be configured in user fuses. scfw should then dynamically adjust the RAM size according to the fuse settings. Is there an example for such an approach?

0 Kudos
Reply
1 Solution
1,838 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

No this is not possible, please note that ROM code will read and execute the SCFW, this will include the DDR initialization. Also, we do not have such approach.

Best regards,
Aldo.

View solution in original post

0 Kudos
Reply
1 Reply
1,839 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

No this is not possible, please note that ROM code will read and execute the SCFW, this will include the DDR initialization. Also, we do not have such approach.

Best regards,
Aldo.

0 Kudos
Reply