iMX8QM MIPI DSI Resolution

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX8QM MIPI DSI Resolution

跳至解决方案
1,188 次查看
dvorak-legend
Contributor I

I'm trying to run a 1440x1440 display from the MIPI DSI output of the i.MX8QM. The datasheet says the max resolution is 1080p60, but the data rate of 1080p60 and 1440x1440 at 60fps is exactly the same. Is this possible, or is there some other hardware limitation? Or is it a better idea to use the HDMI output with a HDMI to MIPI IC/FPGA?

0 项奖励
回复
1 解答
1,177 次查看
igorpadykov
NXP Employee
NXP Employee

Hi dvorak-legend

 

from hardware point of view there are no limitations, however there may be limitations

from driver as it selects working mode automatically. For example of usage of various LCDs

one can look on below link

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8QXP-MEK-Display-Selection-Guide/ta...

and drivers description in  i.MX Linux Reference Manual​

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,178 次查看
igorpadykov
NXP Employee
NXP Employee

Hi dvorak-legend

 

from hardware point of view there are no limitations, however there may be limitations

from driver as it selects working mode automatically. For example of usage of various LCDs

one can look on below link

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8QXP-MEK-Display-Selection-Guide/ta...

and drivers description in  i.MX Linux Reference Manual​

 

Best regards
igor

0 项奖励
回复