iMX8QM MIPI DSI Resolution

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8QM MIPI DSI Resolution

Jump to solution
1,076 Views
dvorak-legend
Contributor I

I'm trying to run a 1440x1440 display from the MIPI DSI output of the i.MX8QM. The datasheet says the max resolution is 1080p60, but the data rate of 1080p60 and 1440x1440 at 60fps is exactly the same. Is this possible, or is there some other hardware limitation? Or is it a better idea to use the HDMI output with a HDMI to MIPI IC/FPGA?

0 Kudos
Reply
1 Solution
1,065 Views
igorpadykov
NXP Employee
NXP Employee

Hi dvorak-legend

 

from hardware point of view there are no limitations, however there may be limitations

from driver as it selects working mode automatically. For example of usage of various LCDs

one can look on below link

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8QXP-MEK-Display-Selection-Guide/ta...

and drivers description in  i.MX Linux Reference Manual​

 

Best regards
igor

View solution in original post

0 Kudos
Reply
1 Reply
1,066 Views
igorpadykov
NXP Employee
NXP Employee

Hi dvorak-legend

 

from hardware point of view there are no limitations, however there may be limitations

from driver as it selects working mode automatically. For example of usage of various LCDs

one can look on below link

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8QXP-MEK-Display-Selection-Guide/ta...

and drivers description in  i.MX Linux Reference Manual​

 

Best regards
igor

0 Kudos
Reply