iMX8QM MIPI DSI Resolution

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8QM MIPI DSI Resolution

ソリューションへジャンプ
2,256件の閲覧回数
dvorak-legend
Contributor I

I'm trying to run a 1440x1440 display from the MIPI DSI output of the i.MX8QM. The datasheet says the max resolution is 1080p60, but the data rate of 1080p60 and 1440x1440 at 60fps is exactly the same. Is this possible, or is there some other hardware limitation? Or is it a better idea to use the HDMI output with a HDMI to MIPI IC/FPGA?

0 件の賞賛
返信
1 解決策
2,245件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi dvorak-legend

 

from hardware point of view there are no limitations, however there may be limitations

from driver as it selects working mode automatically. For example of usage of various LCDs

one can look on below link

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8QXP-MEK-Display-Selection-Guide/ta...

and drivers description in  i.MX Linux Reference Manual​

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,246件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi dvorak-legend

 

from hardware point of view there are no limitations, however there may be limitations

from driver as it selects working mode automatically. For example of usage of various LCDs

one can look on below link

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8QXP-MEK-Display-Selection-Guide/ta...

and drivers description in  i.MX Linux Reference Manual​

 

Best regards
igor

0 件の賞賛
返信