iMX8QM HDMI RX and MIPI-CSI Media issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8QM HDMI RX and MIPI-CSI Media issue

2,804 Views
prashanthkumar
Contributor II

Hi,

We are working on iMX8QM custom board (B0  CPU) with 4.14.98 Kernel BSP.

Here, both HDMI-RX and MIPI-CSI (OV5640 Camera) are working individually. We used following reference MEK DTS files,

arch/arm64/boot/dts/freescale/fsl-imx8qm-mek-ov5640.dts -------- For MIPI-CSI ov5640 camera

arch/arm64/boot/dts/freescale/fsl-imx8qm-mek-hdmi-in.dts -------- For HDMI RX

While cconfiguring both HDMI-RX and MIPI-CSI nodes in DTS file, the '/dev/videox' nodes are not generating in file system.

The DTS configuration as below,

/* Multimedia: Image Sensing Interface */
&isi_0 {
        status = "okay";
};

&isi_1 {
        status = "okay";
};

/* HDMI: HDMI-RX */
&isi_2 {
        interface = <4 0 2>;  /* <Input MIPI_VCx Output>
                                Input:  0-DC0, 1-DC1, 2-MIPI CSI0, 3-MIPI CSI1, 4-HDMI, 5-MEM
                                VCx:    0-VC0, 1-VC1, 2-VC2, 3-VC3, MIPI CSI only
                                Output: 0-DC0, 1-DC1, 2-MEM */
         status = "okay";
};

&isi_3 {
        /* For HDMI RX 4K chain buf */
        interface = <4 0 2>;
        status = "okay";
};

&isi_4 {
        status = "okay";
};

&isi_5 {
        status = "okay";
};

&isi_6 {
        status = "okay";
};

&isi_7 {
        status = "okay";
};

Is this configuration correct? Is  it possible to configure both HDMI-RX and MIPI-CSI (OV5640 Camera) simultaneously in DTS file?

Best Regards,

Prashanth Kumar K

0 Kudos
Reply
2 Replies

2,462 Views
jiangyaqiang
Senior Contributor I

HI  prashanth:

I got the same problem, have you fixed it ?

0 Kudos
Reply

2,462 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Please take a look to this app note

AN5125,

and also take a look to this presentation

Device Tree Made Easy

This may be helpful for you

 

Unfortunately the i.MX8X family is not officially supported yet, please note that i.MX8QM processor is still in pre-production stage, sorry for the inconvenience and the problems this may cause.

 

Thank you for your understanding,

Best regards,
Aldo.

0 Kudos
Reply