iMX8QM HDMI RX and MIPI-CSI Media issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8QM HDMI RX and MIPI-CSI Media issue

2,802件の閲覧回数
prashanthkumar
Contributor II

Hi,

We are working on iMX8QM custom board (B0  CPU) with 4.14.98 Kernel BSP.

Here, both HDMI-RX and MIPI-CSI (OV5640 Camera) are working individually. We used following reference MEK DTS files,

arch/arm64/boot/dts/freescale/fsl-imx8qm-mek-ov5640.dts -------- For MIPI-CSI ov5640 camera

arch/arm64/boot/dts/freescale/fsl-imx8qm-mek-hdmi-in.dts -------- For HDMI RX

While cconfiguring both HDMI-RX and MIPI-CSI nodes in DTS file, the '/dev/videox' nodes are not generating in file system.

The DTS configuration as below,

/* Multimedia: Image Sensing Interface */
&isi_0 {
        status = "okay";
};

&isi_1 {
        status = "okay";
};

/* HDMI: HDMI-RX */
&isi_2 {
        interface = <4 0 2>;  /* <Input MIPI_VCx Output>
                                Input:  0-DC0, 1-DC1, 2-MIPI CSI0, 3-MIPI CSI1, 4-HDMI, 5-MEM
                                VCx:    0-VC0, 1-VC1, 2-VC2, 3-VC3, MIPI CSI only
                                Output: 0-DC0, 1-DC1, 2-MEM */
         status = "okay";
};

&isi_3 {
        /* For HDMI RX 4K chain buf */
        interface = <4 0 2>;
        status = "okay";
};

&isi_4 {
        status = "okay";
};

&isi_5 {
        status = "okay";
};

&isi_6 {
        status = "okay";
};

&isi_7 {
        status = "okay";
};

Is this configuration correct? Is  it possible to configure both HDMI-RX and MIPI-CSI (OV5640 Camera) simultaneously in DTS file?

Best Regards,

Prashanth Kumar K

0 件の賞賛
返信
2 返答(返信)

2,460件の閲覧回数
jiangyaqiang
Senior Contributor I

HI  prashanth:

I got the same problem, have you fixed it ?

0 件の賞賛
返信

2,460件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Please take a look to this app note

AN5125,

and also take a look to this presentation

Device Tree Made Easy

This may be helpful for you

 

Unfortunately the i.MX8X family is not officially supported yet, please note that i.MX8QM processor is still in pre-production stage, sorry for the inconvenience and the problems this may cause.

 

Thank you for your understanding,

Best regards,
Aldo.

0 件の賞賛
返信