iMX8QM Display Port (DP) Bring up Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8QM Display Port (DP) Bring up Issue

2,701件の閲覧回数
prashanthkumar
Contributor II

Hi,

We are working on iMX8QM custom board (B0 CPU) with 4.14.98 Kernel BSP.
The DP(Display Port) interface is crashing while booting.

We tested the same with iMX8QM ARM2 LPDDR4 CPU Validation Board, in that also facing same issue.
We used below DTS file as reference for DP support.

arch/arm64/boot/dts/freescale/fsl-imx8qm-lpddr4-arm2-dp.dts

The boot log is attached for your reference.

Kindly support us to resolve above issue as soon as possible.

Best Regards,

Prashanth Kumar K

0 件の賞賛
返信
3 返答(返信)

2,444件の閲覧回数
prashanthkumar
Contributor II

Hi Igor,

The release notes Linux L4.14.98_2.0.0 Documentation

saying as below. Then DP should support it seems.

pastedImage_1.png

Is there any additional DTS configuration required for DP support?

Best Regards,

Prashanth Kumar K

0 件の賞賛
返信

2,444件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Prashanth 

document shows "supports HDMI", not DP.

Also this is preprduction part with limited support.

Best regards
igor

0 件の賞賛
返信

2,444件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Prashanth

Release Notes document from Linux L4.14.98_2.0.0 Documentation

shows supported functionalities, seems iMX8QM Display Port (DP) is not supported.

One can apply to local nxp office to try get support on that case.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信