iMX8MQ evk with adv7535 no weston ui

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8MQ evk with adv7535 no weston ui

ソリューションへジャンプ
3,558件の閲覧回数
charleshuang
Senior Contributor II

Hi

Yocto zeus 5.4.70

I use imx8mq evk board and adv7535 bridge ic, but I can’t see the weston ui after booting up

I execute the following command then get weston service failed

root@imx8mqevk:~# systemctl -a | grep weston
* weston@root.service loaded failed failed Weston Wayland Compositor (on tty7)

Is this known issue?

ラベル(1)
0 件の賞賛
返信
1 解決策
3,515件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

You need change card from card0 to card1 in weston.ini

 

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,551件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Can you attach your boot and kernel log?

0 件の賞賛
返信
3,532件の閲覧回数
charleshuang
Senior Contributor II

The attached is log file

thanks

0 件の賞賛
返信
3,527件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Which kind of images your are using? imx-image-multimedia? or imx-image-full

0 件の賞賛
返信
3,525件の閲覧回数
charleshuang
Senior Contributor II

We use imx-image-full

thanks

0 件の賞賛
返信
3,516件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

You need change card from card0 to card1 in weston.ini

 

0 件の賞賛
返信