iMX8MP dual camera with ISP - update mi_mp_y_pic_width error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8MP dual camera with ISP - update mi_mp_y_pic_width error

1,577件の閲覧回数
GreatForest
Contributor I

Hello all:

I'm porting two ov4689 cameras to the i.MX 8MP board. (isp-imx-4.2.2.11.0 and isp-vvcam_imx_5.4.70_2.3.2)

Now channel 1 can get the image data, but channel 2 failed to get the data.

Here is the command to get the image, and the log of isp_media_server.

gst-launch-1.0 v4l2src device=/dev/video1 num-buffers=1 ! video/x-raw,width=1280,height=720,framerate=60/1,format=YUY2 ! jpegenc ! filesink location=frame.jpg

GreatForest_0-1667790180614.png

In the red box is an error message. The normal execution message for channel 1 is wdr3 res: 1280 720, but I don't know why channel 2 is 0 0.

Can somebody, please help me on how I can make this work? Thanks in advance !

 

Regards,

Forest.

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,541件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
which dtb do you use?
0 件の賞賛
返信

1,534件の閲覧回数
GreatForest
Contributor I

The attachment is the device tree file I used.

The following is the content of myd-jx8mp-dual-ov4689.dts.

#include "myd-jx8mp-base.dts"

&i2c2 {
	/delete-node/ov5640_mipi@3c;

	ov4689_0: ov4689_mipi@36 {
		compatible = "ovti,ov4689";
		reg = <0x36>;
		pinctrl-names = "default";
		pinctrl-0 = <&pinctrl_csi0_pwn>, <&pinctrl_csi0_rst>,<&pinctrl_io0_pwn>;
		clocks = <&clk IMX8MP_CLK_IPP_DO_CLKO2>;
		clock-names = "csi_mclk";
		assigned-clocks = <&clk IMX8MP_CLK_IPP_DO_CLKO2>;
		assigned-clock-parents = <&clk IMX8MP_CLK_24M>;
		assigned-clock-rates = <24000000>;
		csi_id = <0>;
		pwn-gpios = <&gpio2 11 GPIO_ACTIVE_HIGH>;
		rst-gpios = <&gpio1 6 GPIO_ACTIVE_LOW>;
		mclk = <24000000>;
		mclk_source = <0>;
		mipi_csi;
		status = "okay";

		port {
			ov4689_mipi_0_ep: endpoint {
				remote-endpoint = <&mipi_csi0_ep>;
				data-lanes = <1 2 3 4>;
				clock-lanes = <0>;
			};
		};
	};
};

&i2c3 {
	/delete-node/ov5640_mipi@3c;

	ov4689_1: ov4689_mipi@36 {
		compatible = "ovti,ov4689";
		reg = <0x36>;
		pinctrl-names = "default";
		pinctrl-0 = <&pinctrl_csi1_pwn>, <&pinctrl_csi1_rst>,<&pinctrl_io1_pwn>;
		clocks = <&clk IMX8MP_CLK_IPP_DO_CLKO2>;
		clock-names = "csi_mclk";
		assigned-clocks = <&clk IMX8MP_CLK_IPP_DO_CLKO2>;
		assigned-clock-parents = <&clk IMX8MP_CLK_24M>;
		assigned-clock-rates = <24000000>;
		csi_id = <1>;
		pwn-gpios = <&gpio2 8 GPIO_ACTIVE_HIGH>;
		rst-gpios = <&gpio2 7 GPIO_ACTIVE_LOW>;
		mclk = <24000000>;
		mclk_source = <0>;
		mipi_csi;
		status = "okay";

		port {
			ov4689_mipi_1_ep: endpoint {
				remote-endpoint = <&mipi_csi1_ep>;
				data-lanes = <1 2 3 4>;
				clock-lanes = <0>;
			};
		};
	};
};

&cameradev {
	status = "okay";
};

&isi_0 {
	status = "disabled";
};

&isi_1 {
	status = "disabled";
};

&isp_0 {
	status = "okay";
};

&isp_1 {
	status = "okay";
};

&dewarp {
	status = "okay";
};

&mipi_csi_0 {
	status = "okay";

	port@0 {
		reg = <0>;
		mipi_csi0_ep: endpoint {
			remote-endpoint = <&ov4689_mipi_0_ep>;
			data-lanes = <4>;
			csis-hs-settle = <13>;
			csis-clk-settle = <2>;
			csis-wclk;
		};
	};
};

&mipi_csi_1 {
	status = "okay";

	port@1 {
		reg = <1>;
		mipi_csi1_ep: endpoint {
			remote-endpoint = <&ov4689_mipi_1_ep>;
			data-lanes = <4>;
			csis-hs-settle = <13>;
			csis-clk-settle = <2>;
			csis-wclk;
		};
	};
};

 

At present, I find the problem is that the isp driver failed to write a value to the register.

GreatForest_0-1668502032027.png

 

0 件の賞賛
返信

1,496件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

if you disable isp0, does it isp1 work? you can check the logfile if your board detect and link the ov4689 by isp1 or not

0 件の賞賛
返信