iMX8MP - WebGPU has been disabled via blocklist or the command line

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX8MP - WebGPU has been disabled via blocklist or the command line

跳至解决方案
1,777 次查看
vix
Contributor III

From chromium v117 running on iMX8MP I see the following item in the chrome://gpu page:

  • WebGPU has been disabled via blocklist or the command line.

Disabled Features: webgpu

Is this expected?

I see here some possible reasons, but I don't know which ones apply to the iMX8MP hardware architecture.

Should I pass

--enable-unsafe-webgpu

command line parameter to chromium?

 

Or is this feature unsupported on the iMX8MP hardware?

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
1,744 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 项奖励
回复
3 回复数
1,763 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Currently WebGPU are not supported by MX8MP in latest BSP, but is pure software.

Regards

0 项奖励
回复
1,749 次查看
vix
Contributor III

Hi @Bio_TICFSL 

do you mean that even with the flags suggested by your colleague here, the implementation is full software?

0 项奖励
回复
1,745 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

That;s correct!

0 项奖励
回复