iMX8MP - WebGPU has been disabled via blocklist or the command line

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8MP - WebGPU has been disabled via blocklist or the command line

ソリューションへジャンプ
1,408件の閲覧回数
vix
Contributor III

From chromium v117 running on iMX8MP I see the following item in the chrome://gpu page:

  • WebGPU has been disabled via blocklist or the command line.

Disabled Features: webgpu

Is this expected?

I see here some possible reasons, but I don't know which ones apply to the iMX8MP hardware architecture.

Should I pass

--enable-unsafe-webgpu

command line parameter to chromium?

 

Or is this feature unsupported on the iMX8MP hardware?

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,375件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
3 返答(返信)
1,394件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Currently WebGPU are not supported by MX8MP in latest BSP, but is pure software.

Regards

0 件の賞賛
返信
1,380件の閲覧回数
vix
Contributor III

Hi @Bio_TICFSL 

do you mean that even with the flags suggested by your colleague here, the implementation is full software?

0 件の賞賛
返信
1,376件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

That;s correct!

0 件の賞賛
返信