iMX8MP Software SDP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8MP Software SDP

1,765件の閲覧回数
Wobaffet
Senior Contributor I

Hello,

We’re working on configuring our custom board to enter Serial Download Mode (SDP) via software, without using a physical switch, as the USB port will function solely in host mode in the final product. While it seems feasible through Fastboot, the available instructions aren’t entirely clear.

Our aim is for the device to detect a USB flash drive when plugged in, verify the integrity of an update image on the drive, reboot, flash the image, and then boot from the updated firmware.

Does NXP have a recommended workflow or user guide for achieving this process?

Thanks!

Best Regards.

0 件の賞賛
返信
3 返答(返信)

1,709件の閲覧回数
Wobaffet
Senior Contributor I

Reminder, we need a working case for the imx8mp sw update.

0 件の賞賛
返信

1,733件の閲覧回数
Wobaffet
Senior Contributor I

I don't see any recommendations regarding the update on that document.

0 件の賞賛
返信

1,747件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

One can download the Yocto User Guide document for the BSP you are working on.

Regards

0 件の賞賛
返信