iMX8MP Software SDP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX8MP Software SDP

1,755 次查看
Wobaffet
Senior Contributor I

Hello,

We’re working on configuring our custom board to enter Serial Download Mode (SDP) via software, without using a physical switch, as the USB port will function solely in host mode in the final product. While it seems feasible through Fastboot, the available instructions aren’t entirely clear.

Our aim is for the device to detect a USB flash drive when plugged in, verify the integrity of an update image on the drive, reboot, flash the image, and then boot from the updated firmware.

Does NXP have a recommended workflow or user guide for achieving this process?

Thanks!

Best Regards.

0 项奖励
回复
3 回复数

1,699 次查看
Wobaffet
Senior Contributor I

Reminder, we need a working case for the imx8mp sw update.

0 项奖励
回复

1,723 次查看
Wobaffet
Senior Contributor I

I don't see any recommendations regarding the update on that document.

0 项奖励
回复

1,737 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

One can download the Yocto User Guide document for the BSP you are working on.

Regards

0 项奖励
回复