iMX8MP Software SDP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8MP Software SDP

1,769 Views
Wobaffet
Senior Contributor I

Hello,

We’re working on configuring our custom board to enter Serial Download Mode (SDP) via software, without using a physical switch, as the USB port will function solely in host mode in the final product. While it seems feasible through Fastboot, the available instructions aren’t entirely clear.

Our aim is for the device to detect a USB flash drive when plugged in, verify the integrity of an update image on the drive, reboot, flash the image, and then boot from the updated firmware.

Does NXP have a recommended workflow or user guide for achieving this process?

Thanks!

Best Regards.

0 Kudos
Reply
3 Replies

1,713 Views
Wobaffet
Senior Contributor I

Reminder, we need a working case for the imx8mp sw update.

0 Kudos
Reply

1,737 Views
Wobaffet
Senior Contributor I

I don't see any recommendations regarding the update on that document.

0 Kudos
Reply

1,751 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

One can download the Yocto User Guide document for the BSP you are working on.

Regards

0 Kudos
Reply