[iMX8MP] DDR4 data bit/byte swapping

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[iMX8MP] DDR4 data bit/byte swapping

3,872件の閲覧回数
khang_letruong
Senior Contributor III

Dear Community,

We are about to design our custom iMX8M Plus based CPU board. We will use the same DDR4 memory (MT40A512M16LY-062E) as in the reference design of iMX8M Mini EVK (8MMINID4-EVK) but with half of capacity (8Gb or 1GB).

In the mentioned reference design, there seems to be bit-swapping of data lines between the DDRAM and the iMX8M Mini  :

ddr4-bit-swapping.png

We also need to apply certain bit swapping to optimize the PCB layout and our own bit swapping would be different from above reference design. Therefore, I would like to know where to find the rules of DDR data bit/byte swapping applied for iMX8M Plus, please ? I found following article and application note (AN5097) which seem to be relevant : https://community.nxp.com/t5/Layerscape/AN5097-DDR4-Layout-Checklist-Clarification-for-LS1028A/td-p/...

AN5097 :

ddr4-bitswapping-27.png

ddr4-bitswapping-48.png

I would like to know if above rules should also be applied for the iMX8M Plus ?

Last question, what/where would take into account this bit swapping so that the DDRAM could work correctly : DDR RPA for the timing code generation or else where in u-Boot, please ?

Thanks in advance and best regards,

Khang

ラベル(1)
0 件の賞賛
返信
1 返信

3,852件の閲覧回数
khang_letruong
Senior Contributor III

Hi again, CC : @weidong_sun ,

I found the following discussion in which you said  :

For DDR4, there is no restriction on the exchange of data bits, as you can see in this design files.

How can I interpret above statement correctly (i.e how can I configure this swapping correctly), please ? Seeing that there's no explicit BoardDataBusConfig tab in the MX8M_Plus_DDR4_RPA_v5.xlsx, but in MX8M_Plus_LPDDR4_RPA_v7.xlsx as below :

LPDDR4-BoardDataBusConfig.png

Thanks and best regards,

Khang.

 

 

 

0 件の賞賛
返信