iMX8MM Firmware does not load automatically

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX8MM Firmware does not load automatically

跳至解决方案
2,936 次查看
raajeshk88
Contributor III

The SDMA firmware does not load automatically. I can find the /lib/firmware/imx/sdma/sdma-imx7d.bin and the dts points to the exact location.
The udev script needs to be implemented to load the firmware seperately which is executed after the default timeout of 60 secs. Am I missing any config in kernel? I could not see the same issue with iMX8MM EVK eval kit with IMX image with 4.14. 

标签 (1)
0 项奖励
回复
1 解答
2,881 次查看
raajeshk88
Contributor III

Hi Igor,

      The issue is actually with FW_USER_HELPER_FALLBACK is enabled in kernel config. And i also made the imx-sdma as module. Thanks

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,882 次查看
raajeshk88
Contributor III

Hi Igor,

      The issue is actually with FW_USER_HELPER_FALLBACK is enabled in kernel config. And i also made the imx-sdma as module. Thanks

0 项奖励
回复
2,912 次查看
raajeshk88
Contributor III

Hi Igor,

          Let me try this. But we are facing similar issue with all firmware loading. We need to write a separate udev to load them/ Does FW_HELPER_FALLBACK is needed

0 项奖励
回复
2,923 次查看
igorpadykov
NXP Employee
NXP Employee

Hi raajeshk88

 

one can try suggestions provided on

https://community.nxp.com/t5/i-MX-Processors/i-MX7S-hangs-with-sumo-4-14-78-1-0-0-ga-when-loading-sd...

 

Best regards
igor

0 项奖励
回复