iMX8MM Firmware does not load automatically

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8MM Firmware does not load automatically

Jump to solution
2,937 Views
raajeshk88
Contributor III

The SDMA firmware does not load automatically. I can find the /lib/firmware/imx/sdma/sdma-imx7d.bin and the dts points to the exact location.
The udev script needs to be implemented to load the firmware seperately which is executed after the default timeout of 60 secs. Am I missing any config in kernel? I could not see the same issue with iMX8MM EVK eval kit with IMX image with 4.14. 

Labels (1)
0 Kudos
Reply
1 Solution
2,882 Views
raajeshk88
Contributor III

Hi Igor,

      The issue is actually with FW_USER_HELPER_FALLBACK is enabled in kernel config. And i also made the imx-sdma as module. Thanks

View solution in original post

0 Kudos
Reply
3 Replies
2,883 Views
raajeshk88
Contributor III

Hi Igor,

      The issue is actually with FW_USER_HELPER_FALLBACK is enabled in kernel config. And i also made the imx-sdma as module. Thanks

0 Kudos
Reply
2,913 Views
raajeshk88
Contributor III

Hi Igor,

          Let me try this. But we are facing similar issue with all firmware loading. We need to write a separate udev to load them/ Does FW_HELPER_FALLBACK is needed

0 Kudos
Reply
2,924 Views
igorpadykov
NXP Employee
NXP Employee

Hi raajeshk88

 

one can try suggestions provided on

https://community.nxp.com/t5/i-MX-Processors/i-MX7S-hangs-with-sumo-4-14-78-1-0-0-ga-when-loading-sd...

 

Best regards
igor

0 Kudos
Reply