iMX8MM - Cortex M4 Debug Console

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8MM - Cortex M4 Debug Console

ソリューションへジャンプ
1,772件の閲覧回数
c_guerr
Contributor III

 

 

Hi, 


I try to run many exemples provided by the MCUXpresso of Cortex M4 Applications such as:

- RPMSG

- GPT.

Both examples works properly when I run them from U-Boot. For the GPT i see the counter value.
But once the kernel is booted, I have no more messages from the UART I selected for Cortex M4.

For the GPT Problems i thought the original cause would be the same as here: https://community.nxp.com/t5/i-MX-Processors/GPT-capture-sample-on-M4-seems-to-hang-on-Linux-boot/m-...

But I have the same behavior using RPMsg examples.

The ping-pong examples works well in the linux side, getting messages from the Cortex M4. But no UART messages.

Cortex M4 use UART3 and Cortex A53 use UART4.

 

On device tree i've done the following:

 

&ecspi1 {
        status = "disabled";
};

&i2c4 {
        status = "disabled";
};

&pwm3 {
        status = "disabled";
};

&rpmsg{
        /*
         * 64K for one rpmsg instance:
         * --0x40000000~0x4000ffff: pingpong
         */
        vdev-nums = <1>;
        reg = <0x0 0x40000000 0x0 0x10000>;
        memory-region = <&vdevbuffer>;
        status = "okay";
};

&sdma1{
        status = "disabled";
};

&uart3 {
        status = "disabled";
};

 


Disabled ecspi1 as it uses the same pinmuxing of the UART3 and sure, disabling UART3 also.

I've followed the advices of the link show above by reading on registers but i see that UART3 is enabled. In /sys/firmware/devicetree... and so on, uart3 is disabled. So the register have been updated by the CORTEX M4 I guess.

What do you suggest?

Thanks in advance!

 

 

0 件の賞賛
返信
1 解決策
1,719件の閲覧回数
c_guerr
Contributor III

I found out.

The GPIO5_IO27 was used by the PCIE0 which use the same pad as UART3 RXD.

Sorry for bothering.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,720件の閲覧回数
c_guerr
Contributor III

I found out.

The GPIO5_IO27 was used by the PCIE0 which use the same pad as UART3 RXD.

Sorry for bothering.

0 件の賞賛
返信