iMX8M Nano :- U-boot and Kernel Source Download

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M Nano :- U-boot and Kernel Source Download

Jump to solution
6,894 Views
milav_soni
Contributor III

 

Hello Guys,

I want to download IMX U-boot and Kernel Source for imx8m nano EVK.

So from where am i download the standalone sources for standalone build uboot and kernel for the imx8mnano evk?

can you please provide me link?

I found following link as i am searching on google. is it okay to download it?

Which Linux kernel and u-boot version are download for my build configuration.

Link :- https://source.codeaurora.org/external/imx 

Below is my build Configuration for the same.

 

Build Configuration:
BB_VERSION           = "1.44.0"
BUILD_SYS            = "x86_64-linux"
NATIVELSBSTRING      = "ubuntu-19.04"
TARGET_SYS           = "aarch64-poky-linux"
MACHINE              = "imx8mnevk"
DISTRO               = "fsl-imx-wayland"
DISTRO_VERSION       = "5.4-zeus"
TUNE_FEATURES        = "aarch64 cortexa53 crc crypto"
TARGET_FPU           = ""
meta                 
meta-poky            = "HEAD:5408e48d374fc741fa46b57ddfd8a537843bda6f"
meta-oe              
meta-multimedia      
meta-python          = "HEAD:2b5dd1eb81cd08bc065bc76125f2856e9383e98b"
meta-freescale       = "HEAD:14f1a630a47375432f93c556927b879b51d84c4e"
meta-freescale-3rdparty = "HEAD:dbcc686f52c3c84db8cb86aa8973a4e373651b98"
meta-freescale-distro = "HEAD:ca27d12e4964d1336e662bcc60184bbff526c857"
meta-bsp             
meta-sdk             
meta-ml              = "HEAD:780b023a4c77ac9c0011d858ad377f4a9593bfea"
meta-nxp-demo-experience = "HEAD:c7263d9f3cc7bbf44e7164ffeda494cf283d3dec"
meta-browser         = "HEAD:ee3be3b5986a4aa0e73df2204a625ae1fe5df37e"
meta-rust            = "HEAD:7f235b6f8973cc5269448375f2a8f9867bb2a369"
meta-clang           = "HEAD:711e593d5984aad3bf35c51b7ac4482982bc16c7"
meta-gnome           
meta-networking      
meta-filesystems     = "HEAD:2b5dd1eb81cd08bc065bc76125f2856e9383e98b"
meta-qt5             = "HEAD:5144a99a696a8a72c0765ea0e8be8ceafaa78f85"
meta-python2         = "HEAD:4400f9155ec193d028208cf0c66aeed2ba2b00ab"

 

I have already generate SDK environment in my sdk path by running following script file.

 

$./fsl-imx-wayland-glibc-x86_64-core-image-minimal-aarch64-imx8mnevk-toolchain-5.4-zeus.sh

 

Please help me out.

Thank You

 

Labels (2)
0 Kudos
Reply
1 Solution
6,870 Views
joanxie
NXP TechSupport
NXP TechSupport

if you just want to refer to the source code, you don't need to download in your ubuntu, you can refer to the link as below:

kernel:

https://source.codeaurora.org/external/imx/linux-imx/

uboot:

https://source.codeaurora.org/external/imx/uboot-imx/

View solution in original post

0 Kudos
Reply
3 Replies
6,884 Views
joanxie
NXP TechSupport
NXP TechSupport

if you need source code not pre-built images, you can refer to the enclosed yocto user guide, first you need to install ubuntu 18.04, then download and built the source code step by step according to the enclosed file

 

0 Kudos
Reply
6,881 Views
milav_soni
Contributor III

 

Hello @joanxie 

I have Yocto Project User Guide.

I need linux-imx and uboot-imx source. 

so for that i need reference link.

Thank you

0 Kudos
Reply
6,871 Views
joanxie
NXP TechSupport
NXP TechSupport

if you just want to refer to the source code, you don't need to download in your ubuntu, you can refer to the link as below:

kernel:

https://source.codeaurora.org/external/imx/linux-imx/

uboot:

https://source.codeaurora.org/external/imx/uboot-imx/

0 Kudos
Reply