Hello Guys,
I want to download IMX U-boot and Kernel Source for imx8m nano EVK.
So from where am i download the standalone sources for standalone build uboot and kernel for the imx8mnano evk?
can you please provide me link?
I found following link as i am searching on google. is it okay to download it?
Which Linux kernel and u-boot version are download for my build configuration.
Link :- https://source.codeaurora.org/external/imx
Below is my build Configuration for the same.
Build Configuration:
BB_VERSION = "1.44.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-19.04"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8mnevk"
DISTRO = "fsl-imx-wayland"
DISTRO_VERSION = "5.4-zeus"
TUNE_FEATURES = "aarch64 cortexa53 crc crypto"
TARGET_FPU = ""
meta
meta-poky = "HEAD:5408e48d374fc741fa46b57ddfd8a537843bda6f"
meta-oe
meta-multimedia
meta-python = "HEAD:2b5dd1eb81cd08bc065bc76125f2856e9383e98b"
meta-freescale = "HEAD:14f1a630a47375432f93c556927b879b51d84c4e"
meta-freescale-3rdparty = "HEAD:dbcc686f52c3c84db8cb86aa8973a4e373651b98"
meta-freescale-distro = "HEAD:ca27d12e4964d1336e662bcc60184bbff526c857"
meta-bsp
meta-sdk
meta-ml = "HEAD:780b023a4c77ac9c0011d858ad377f4a9593bfea"
meta-nxp-demo-experience = "HEAD:c7263d9f3cc7bbf44e7164ffeda494cf283d3dec"
meta-browser = "HEAD:ee3be3b5986a4aa0e73df2204a625ae1fe5df37e"
meta-rust = "HEAD:7f235b6f8973cc5269448375f2a8f9867bb2a369"
meta-clang = "HEAD:711e593d5984aad3bf35c51b7ac4482982bc16c7"
meta-gnome
meta-networking
meta-filesystems = "HEAD:2b5dd1eb81cd08bc065bc76125f2856e9383e98b"
meta-qt5 = "HEAD:5144a99a696a8a72c0765ea0e8be8ceafaa78f85"
meta-python2 = "HEAD:4400f9155ec193d028208cf0c66aeed2ba2b00ab"
I have already generate SDK environment in my sdk path by running following script file.
$./fsl-imx-wayland-glibc-x86_64-core-image-minimal-aarch64-imx8mnevk-toolchain-5.4-zeus.sh
Please help me out.
Thank You
解決済! 解決策の投稿を見る。
if you just want to refer to the source code, you don't need to download in your ubuntu, you can refer to the link as below:
kernel:
https://source.codeaurora.org/external/imx/linux-imx/
uboot:
Hello @joanxie
I have Yocto Project User Guide.
I need linux-imx and uboot-imx source.
so for that i need reference link.
Thank you
if you just want to refer to the source code, you don't need to download in your ubuntu, you can refer to the link as below:
kernel:
https://source.codeaurora.org/external/imx/linux-imx/
uboot: