iMX8M Mini Flashing Empty eMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M Mini Flashing Empty eMMC

Jump to solution
3,900 Views
namanthaker
Contributor IV

Hello,

I am planning to use a custom board with IMX8M Mini SoC. This board would have a empty eMMC without any images flashed on it. I want to flash Android images (android_p9.0.0_2.3.0_image_8mmevk) including the bootloaders, Kernel, system, etc images in the blank eMMC on this board.

I have below question regarding the process:
1. Will UUU be enough to flash the empty eMMC? Or is their another method/utility required for flashing an empty eMMC?
2. I am planning to use USB Type C on board for flashing the images from a Linux based PC. Will this connection (USB Type A on PC -> USB type C on board, same as in IMX8M Mini EVK) work for flashing the images or do I need to use JTAG or some other method for first time flashing?

Thanks

0 Kudos
Reply
1 Solution
3,699 Views
igorpadykov
NXP Employee
NXP Employee

Hi Naman

1. UUU will be enough, from sect.5 Programming Images Android™ User's Guide :

"The following download methods can be used to write the Android System Image:
• UUU to download all images to the eMMC/SD card.
• fsl-sdcard-partition.sh to download all images to the SD card.
• fastboot_imx_flashall script to download all images to the eMMC/SD storage."

2. yes it will work, jtag is not needed.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
3,700 Views
igorpadykov
NXP Employee
NXP Employee

Hi Naman

1. UUU will be enough, from sect.5 Programming Images Android™ User's Guide :

"The following download methods can be used to write the Android System Image:
• UUU to download all images to the eMMC/SD card.
• fsl-sdcard-partition.sh to download all images to the SD card.
• fastboot_imx_flashall script to download all images to the eMMC/SD storage."

2. yes it will work, jtag is not needed.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,699 Views
namanthaker
Contributor IV

Hello,

Thank you for your prompt reply.

So just to confirm my understanding, UUU tool will flash an empty eMMC and perform all the provisioning/partitioning ?

Thanks

0 Kudos
Reply
3,699 Views
igorpadykov
NXP Employee
NXP Employee

right.

~igor

0 Kudos
Reply
3,699 Views
namanthaker
Contributor IV

Thank you very much Igor.

0 Kudos
Reply