iMX8 Linux driver for TJA1101

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8 Linux driver for TJA1101

Jump to solution
2,715 Views
tony-atlismv
Contributor III

I would like to know if there is a Linux driver for the NXP TJA1101 automotive Ehternet PHY IC? I am using a iMX8QM MEK with the ADTJA1101-RMII adaptor card but saw in the Linux kernel NET driver tree under the NXP folder that there was no C files supporting the TJA1101. 

So, is there a repository or link where I can find the TJA1101 driver code and either build it as a stand alone Linux module and use "insmod" to instantiate it, or build the driver into the Linux kernel using Yocto? Note that I am using the latest Linux kernel sources from following the latest version of the iMX Yocto Project Users Guide dated 3/2021.

Or, do I have to create my own Linux kernel driver for the TJA1101?

Thanks

0 Kudos
Reply
1 Solution
1 Reply