I would like to know if there is a Linux driver for the NXP TJA1101 automotive Ehternet PHY IC? I am using a iMX8QM MEK with the ADTJA1101-RMII adaptor card but saw in the Linux kernel NET driver tree under the NXP folder that there was no C files supporting the TJA1101.
So, is there a repository or link where I can find the TJA1101 driver code and either build it as a stand alone Linux module and use "insmod" to instantiate it, or build the driver into the Linux kernel using Yocto? Note that I am using the latest Linux kernel sources from following the latest version of the iMX Yocto Project Users Guide dated 3/2021.
Or, do I have to create my own Linux kernel driver for the TJA1101?
Thanks
Solved! Go to Solution.
Hi Tony
one can look at
https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/net/phy/nxp-tja11xx.c?h=lf-5.10.y
nxp linux documentation
Best regards
igor
Hi Tony
one can look at
https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/net/phy/nxp-tja11xx.c?h=lf-5.10.y
nxp linux documentation
Best regards
igor