iMX7D RDC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,970件の閲覧回数
rolfcrapp
Fresh Out Contributor

With the RDC it's possible to assign ressources to the different cores.

Is it possible to assigne interfaces which are on the same gpio bank to different cores?

example:

GPIO4 bank:

-   I2C1 to M4 core

-   I2C2 to A7 core

-   ECSPI1 to A7 Core

-   ECSPI2 to M4 core

all this interface are on the same GPIO bank. But assigned to different cores.

in my understanding, the interface can be assigned as you like, regardless of which gpio bank they are.

only when allocating the GPIO,  one full bank (ex. GPIO4 Bank) at a time must be allocated. However, regardless of the interface.

タグ(3)
0 件の賞賛
返信
1 解決策
2,746件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi rolfcrapp

you are right, the interface can be assigned as you like,

regardless of which gpio bank they are.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,747件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi rolfcrapp

you are right, the interface can be assigned as you like,

regardless of which gpio bank they are.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,668件の閲覧回数
cyc583723081
Contributor I

您好!

     请问每个GPIO引脚都可以单独分配给不同的核心吗?还是说在作为GPIO时,只能将gpiox bank整组分配?

0 件の賞賛
返信