Request for connection of 1pps from a GNSS module to i.MX8 processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Request for connection of 1pps from a GNSS module to i.MX8 processor

2,077件の閲覧回数
puneethkumar
Contributor III
Dear Team, We are using i.mx8 processor , we want to connect a 1PPS signal output from GPS module to the processor for time synchronization. Processor: i.MX8 DXL Please let us know to which pin of i.MX8 processor should i connect the 1PPS signal. Thanks
0 件の賞賛
返信
5 返答(返信)

2,055件の閲覧回数
puneethkumar
Contributor III

Dear igor,

Please confirm whether shared link is for IMX8DXLAEC processor.

background to this question - when I opened the link it was referring to MCU.

Thanks,

Puneeth S Kumar

0 件の賞賛
返信

2,052件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

answer was provided referring to IMX8DXLAEC
( i.MX 8XLite Automotive and Infotainment Applications Processors)

 

Best regards
igor

0 件の賞賛
返信

2,064件の閲覧回数
puneethkumar
Contributor III

Dear Team,

I am referring to IMX8DXLAEC ( i.MX 8XLite Automotive and Infotainment Applications Processors)

Please let me know above proposed solution is for the same

Thanks 

0 件の賞賛
返信

2,062件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

answer was provided referring to IMX8DXLAEC.

 

Best regards
igor

0 件の賞賛
返信

2,071件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi puneethkumar

 

it can be connected to M40_TPM0_CH0 signal of M4 TPM module, TPM examples can be
found in M4 SDK_EVAL-MIMX8DXL available on https://mcuxpresso.nxp.com/en/welcome

 

Best regards
igor

0 件の賞賛
返信