iMX7D 16-bit DDR3 Implementation Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX7D 16-bit DDR3 Implementation Issue

Jump to solution
1,756 Views
x10
Contributor V

Hi, NXP team

Does iMX7D support 16-bit DDR3 implementation? In RM DDRC_MSTR[13:12] = DATA_BUS_WIDTH = 2'b01: Half DQ bus width to SDRAM-DRAM_DATA[15:0], it seems that DDRC can work with 16-bit DDR3 chip, but it doesn't work with my test. I just want to make sure if iMX7D DDRC can work with 16-bit DDR3 or not, otherwise something wrong in my test.

Thanks!

Cheng Shi

 

Labels (2)
0 Kudos
Reply
1 Solution
1,686 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Yes, your understanding is correct.

Best regards.

View solution in original post

0 Kudos
Reply
3 Replies
1,726 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

i.MX7D supports 16/32-bit DDR3L/LPDDR2/LPDDR3-1066 memories.

You can configure this directly in RPA when doing the DDR stress test.

Best regards.

0 Kudos
Reply
1,703 Views
x10
Contributor V

Thanks for quick reply!

As my understanding, the ds file generated by MX7D_DDR3_Register_Programming_Aid_V1_3 can been used to setup 16-bit DDR3(single chip). Is that right?

 

Regards

Cheng Shi

0 Kudos
Reply
1,687 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Yes, your understanding is correct.

Best regards.

0 Kudos
Reply