iMX7 RGMII voltage rating

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX7 RGMII voltage rating

Jump to solution
3,303 Views
justin_hsieh
Contributor II

Dear Team,

Our product is iMX7 plateform with giga ethernet PHY applicatin, and RGMII operation voltage is 3.3V.

We find Ethernet PHY 125MHz clock Max/Min voltage are 3.80835V/-1.02387V,but we can't find the RGMII voltage rating in product spec.

please help check does RGMII clock meet iMX7 RGMII RX Spec.?

RGMII_RX_CLKRGMII_RX_CLK

 

Thks,

Justin

0 Kudos
Reply
1 Solution
3,282 Views
igorpadykov
NXP Employee
NXP Employee

please refer to datasheet

 

1.jpg

 

 

2.jpg

 

 

 

Best regards
igor

View solution in original post

0 Kudos
Reply
3 Replies
3,289 Views
justin_hsieh
Contributor II

Hi igor,

According to RGMII Spec., Tr/Tf must smaller than 0.75ns, we have to increase RX_CLK drive capacity and cause the Max/Min voltage be 3.80835V/-1.02387V.

Can you kindly help to check iMX7 can stand the Max/Min voltage are 3.80835V/-1.02387V or not?

Tks,

Justin

0 Kudos
Reply
3,283 Views
igorpadykov
NXP Employee
NXP Employee

please refer to datasheet

 

1.jpg

 

 

2.jpg

 

 

 

Best regards
igor

0 Kudos
Reply
3,295 Views
igorpadykov
NXP Employee
NXP Employee

Hi justin_hsieh

 

enet voltages can be found in Table 9. Operating ranges

i.MX 7Dual Family of Applications Processors Datasheet

also one can use rgmii example in

Design files, including hardware schematics, Gerbers, and OrCAD files for i.MX 7Dual 

 

Best regards
igor

0 Kudos
Reply