iMX7 RGMII voltage rating

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX7 RGMII voltage rating

ソリューションへジャンプ
3,212件の閲覧回数
justin_hsieh
Contributor II

Dear Team,

Our product is iMX7 plateform with giga ethernet PHY applicatin, and RGMII operation voltage is 3.3V.

We find Ethernet PHY 125MHz clock Max/Min voltage are 3.80835V/-1.02387V,but we can't find the RGMII voltage rating in product spec.

please help check does RGMII clock meet iMX7 RGMII RX Spec.?

RGMII_RX_CLKRGMII_RX_CLK

 

Thks,

Justin

0 件の賞賛
返信
1 解決策
3,191件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

please refer to datasheet

 

1.jpg

 

 

2.jpg

 

 

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,198件の閲覧回数
justin_hsieh
Contributor II

Hi igor,

According to RGMII Spec., Tr/Tf must smaller than 0.75ns, we have to increase RX_CLK drive capacity and cause the Max/Min voltage be 3.80835V/-1.02387V.

Can you kindly help to check iMX7 can stand the Max/Min voltage are 3.80835V/-1.02387V or not?

Tks,

Justin

0 件の賞賛
返信
3,192件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

please refer to datasheet

 

1.jpg

 

 

2.jpg

 

 

 

Best regards
igor

0 件の賞賛
返信
3,204件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi justin_hsieh

 

enet voltages can be found in Table 9. Operating ranges

i.MX 7Dual Family of Applications Processors Datasheet

also one can use rgmii example in

Design files, including hardware schematics, Gerbers, and OrCAD files for i.MX 7Dual 

 

Best regards
igor

0 件の賞賛
返信