iMX6UL - run u-boot from eMMC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX6UL - run u-boot from eMMC

跳至解决方案
4,064 次查看
nickbedbury
Contributor III

I am trying to bring up a custom iMX6UL board booting from eMMC, and encountering some issues. 

I believe eMMC is hooked up properly.  Via JTAG, I can load u-boot.bin (built from uboot-fslc-2017.11, the repo Yocto references) to 0x87800000.  Then u-boot runs and gives me a console, from which eMMC works successfully ("mmc info", etc). 

For production, we are using u-boot and SPL built from this code base:

configs: icore-rqs: Enable falcon mode · Freescale/u-boot-fslc@ca0c3f3 · GitHub 

I have loaded the compiled SPL to address 1kB and u-boot.img to address 69kB, as per the iMX6UL EVK.  I used the command "dd if=SPL of=/dev/mmcblk1 bs=1k seek=1" to program the SPL for example.   When I boot however, I don't see any console.  I assume the SPL would print some message if it ran properly?

Based on scoping the eMMC signals, it looks like the iMX6UL ROM bootloader reads 4kB from the eMMC as described in the reference manual section 8.5.3.  I verified the bytes at 1kB offset into the 4kB block read are the SPL file.

Other than scoping the eMMC signals, is there another way to verify the SPL works properly?  Can I load it via JTAG to SRAM (perhaps address 0x908000?) and mimic a power-up boot?

标签 (1)
0 项奖励
回复
1 解答
3,234 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nick

one can look at gateworks tutorial

ventana/bootloader/falcon-mode – Gateworks 

Also one can test with nxp uboot (guidelines can be found on below link),

however it does not use spl.

i.MX Software|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,235 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nick

one can look at gateworks tutorial

ventana/bootloader/falcon-mode – Gateworks 

Also one can test with nxp uboot (guidelines can be found on below link),

however it does not use spl.

i.MX Software|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,234 次查看
nickbedbury
Contributor III

Thanks Igor.  The nxp uboot you referenced works for me (I booted from eMMC).  I guess it was a problem with the uboot variants I had tried to use.

0 项奖励
回复
3,234 次查看
nickbedbury
Contributor III

As an addendum: I did not use the MMC's boot partitions (/dev/mmcblk1boot0 or /dev/mmcblk1boot1) because I didn't have any way to set "boot_config" as per this post:  https://community.nxp.com/thread/429311

I am convinced the SPL and u-boot need to be in /dev/mmcblk1 (the user area) because it's where the ROM bootloader is reading from.

0 项奖励
回复