iMX6UL - run u-boot from eMMC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6UL - run u-boot from eMMC

ソリューションへジャンプ
5,173件の閲覧回数
nickbedbury
Contributor III

I am trying to bring up a custom iMX6UL board booting from eMMC, and encountering some issues. 

I believe eMMC is hooked up properly.  Via JTAG, I can load u-boot.bin (built from uboot-fslc-2017.11, the repo Yocto references) to 0x87800000.  Then u-boot runs and gives me a console, from which eMMC works successfully ("mmc info", etc). 

For production, we are using u-boot and SPL built from this code base:

configs: icore-rqs: Enable falcon mode · Freescale/u-boot-fslc@ca0c3f3 · GitHub 

I have loaded the compiled SPL to address 1kB and u-boot.img to address 69kB, as per the iMX6UL EVK.  I used the command "dd if=SPL of=/dev/mmcblk1 bs=1k seek=1" to program the SPL for example.   When I boot however, I don't see any console.  I assume the SPL would print some message if it ran properly?

Based on scoping the eMMC signals, it looks like the iMX6UL ROM bootloader reads 4kB from the eMMC as described in the reference manual section 8.5.3.  I verified the bytes at 1kB offset into the 4kB block read are the SPL file.

Other than scoping the eMMC signals, is there another way to verify the SPL works properly?  Can I load it via JTAG to SRAM (perhaps address 0x908000?) and mimic a power-up boot?

ラベル(1)
0 件の賞賛
返信
1 解決策
4,343件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nick

one can look at gateworks tutorial

ventana/bootloader/falcon-mode – Gateworks 

Also one can test with nxp uboot (guidelines can be found on below link),

however it does not use spl.

i.MX Software|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,344件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nick

one can look at gateworks tutorial

ventana/bootloader/falcon-mode – Gateworks 

Also one can test with nxp uboot (guidelines can be found on below link),

however it does not use spl.

i.MX Software|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
4,343件の閲覧回数
nickbedbury
Contributor III

Thanks Igor.  The nxp uboot you referenced works for me (I booted from eMMC).  I guess it was a problem with the uboot variants I had tried to use.

0 件の賞賛
返信
4,343件の閲覧回数
nickbedbury
Contributor III

As an addendum: I did not use the MMC's boot partitions (/dev/mmcblk1boot0 or /dev/mmcblk1boot1) because I didn't have any way to set "boot_config" as per this post:  https://community.nxp.com/thread/429311

I am convinced the SPL and u-boot need to be in /dev/mmcblk1 (the user area) because it's where the ROM bootloader is reading from.

0 件の賞賛
返信