iMX6SoloLite processor schematic/PCB symbol

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6SoloLite processor schematic/PCB symbol

Jump to solution
3,733 Views
Lankor
Contributor I

Can someone from Freescale convert the iMX6SL EVK schematic(SCH-27452_B.DSN) from OrCAD to Altium format? Or convert it into other format that Altium can import. When I tried to import the schematic, it showed "can't recognize the file".

Thanks too much!

Labels (1)
0 Kudos
Reply
1 Solution
3,206 Views
Yuri
NXP Employee
NXP Employee

Please try the enclosed (as result of saving as 16.2 version).

View solution in original post

0 Kudos
Reply
4 Replies
3,207 Views
Yuri
NXP Employee
NXP Employee

Please try the enclosed (as result of saving as 16.2 version).

0 Kudos
Reply
3,206 Views
Lankor
Contributor I

Thank you, Yuri. I can import it into Altium now.

0 Kudos
Reply
3,206 Views
raghavendraanja
Contributor II

Just install the cadence evaluation setup in the system where you have Altium and then import it works.

i have done the translation from .dsn to altium.

3,206 Views
hippo
NXP TechSupport
NXP TechSupport

you can find an OrCAD DSN file saved at version 16.2

version after 16.2 are not supported on Altium. The original one is 16.3