iMX6SoloLite processor schematic/PCB symbol

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6SoloLite processor schematic/PCB symbol

ソリューションへジャンプ
3,834件の閲覧回数
Lankor
Contributor I

Can someone from Freescale convert the iMX6SL EVK schematic(SCH-27452_B.DSN) from OrCAD to Altium format? Or convert it into other format that Altium can import. When I tried to import the schematic, it showed "can't recognize the file".

Thanks too much!

ラベル(1)
0 件の賞賛
返信
1 解決策
3,307件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please try the enclosed (as result of saving as 16.2 version).

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,308件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please try the enclosed (as result of saving as 16.2 version).

0 件の賞賛
返信
3,307件の閲覧回数
Lankor
Contributor I

Thank you, Yuri. I can import it into Altium now.

0 件の賞賛
返信
3,307件の閲覧回数
raghavendraanja
Contributor II

Just install the cadence evaluation setup in the system where you have Altium and then import it works.

i have done the translation from .dsn to altium.

3,307件の閲覧回数
hippo
NXP TechSupport
NXP TechSupport

you can find an OrCAD DSN file saved at version 16.2

version after 16.2 are not supported on Altium. The original one is 16.3