iMX6SL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,102件の閲覧回数
phamhuynh
Contributor II

hi, good day, iMX6SL have support MIPI DBI interface? 

ラベル(1)
0 件の賞賛
返信
1 解決策
2,782件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Strictly speaking, IMX6 SL does not support MIPI display.

The following are supported :

• EPDC (electrophoretic display controller): display controller for E-INK EPD panel

• SPDC (SiPix display controller): display controller for SiPix EPD panel

• LCDIF (LCD interface): 24-bit parallel RGB LCD interface

  Nevertheless, it makes sense to analyze datasheets of i.MX6 and display in more
details for different mode using and timing parameters, perhaps LCDIF of the i.MX6 SL
in MPU mode may be applied with MIPI DBI (parallel).


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,783件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Strictly speaking, IMX6 SL does not support MIPI display.

The following are supported :

• EPDC (electrophoretic display controller): display controller for E-INK EPD panel

• SPDC (SiPix display controller): display controller for SiPix EPD panel

• LCDIF (LCD interface): 24-bit parallel RGB LCD interface

  Nevertheless, it makes sense to analyze datasheets of i.MX6 and display in more
details for different mode using and timing parameters, perhaps LCDIF of the i.MX6 SL
in MPU mode may be applied with MIPI DBI (parallel).


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,782件の閲覧回数
phamhuynh
Contributor II

thank for help :smileyhappy:

0 件の賞賛
返信