i.MX6 Quad reset time in serial downloader mode when WDOG_ENABLE=1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 Quad reset time in serial downloader mode when WDOG_ENABLE=1

ソリューションへジャンプ
1,726件の閲覧回数
m_c
Senior Contributor I

In figure 8-2 USB Boot Flow of IMX6DQRM Rev. 2, it said ARM core will reset if no any activity within 32 seconds when WDOG_ENABLE=1. However, in ERR006282 of IMX6DQCEC Rev. 4. The workaround #2 said, the Watchdog timer begins a 90-second countdown and, if nothing interrupts this process, the part resets.

1. The 32 and 90 seconds. Which one is right?

2. Is this delay time can change or not?

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
1,477件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

1. 90sec

2. yes, from sect.70.5.1.1 IMX6DQRM  :

..The timeout value can be changed at any point..

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,478件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

1. 90sec

2. yes, from sect.70.5.1.1 IMX6DQRM  :

..The timeout value can be changed at any point..

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,477件の閲覧回数
m_c
Senior Contributor I

Is this timeout value will remain after cold reboot (power off, then power on)?

0 件の賞賛
返信