iMX6SDL behaviour before POR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6SDL behaviour before POR

Jump to solution
1,812 Views
mosmos
Contributor I

Hello,

the "Out of reset condition" for GPIO_17 (i.MX6 SDL) is "ALT5 gpio7.GPIO[12] Input 100k pullup".

Is there any documentation for the behaviour of this pin while being in reset-state? (before the PMIC pulls POR high while power-up)

We need this signal as an active-low GPIO-pin, so it must be high in reset-state

Labels (2)
0 Kudos
Reply
1 Solution
1,501 Views
igorpadykov
NXP Employee
NXP Employee

Hi Manuel

assumed that in reset-state the same as after, except:

Table 101. Signals with Differing Before Reset and After Reset States  IMX6SDLCEC

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,502 Views
igorpadykov
NXP Employee
NXP Employee

Hi Manuel

assumed that in reset-state the same as after, except:

Table 101. Signals with Differing Before Reset and After Reset States  IMX6SDLCEC

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply