iMX6Q Type Differences

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX6Q Type Differences

跳至解决方案
2,165 次查看
atillametetured
Contributor V

Hello,

Quick question about the three different versions of the application processors iMX6Q.

Is it only the operational temperature that differs between;

1. i.MX 6Dual/6Quad Applications Processors for Industrial Products

2. i.MX 6Dual/6Quad Applications Processors for Consumer Products

3. i.MX 6Dual/6Quad Automotive and Infotainment Applications Processors

If not only the temperature, what else seperates these three?

Best Regards,

Mete

标签 (2)
1 解答
2,054 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Atilla

all parts share the same modules, so functionality is identical.

Differencies can be in lifetime, check AN4724,25 i.MX 6  Product Usage Lifetime.

Also automotive parts pass factory tests for compliance with automotive

specifications for use in the harsh automotive environment.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,054 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Atilla

all parts share the same modules, so functionality is identical.

Differencies can be in lifetime, check AN4724,25 i.MX 6  Product Usage Lifetime.

Also automotive parts pass factory tests for compliance with automotive

specifications for use in the harsh automotive environment.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,054 次查看
atillametetured
Contributor V

Hi Igor,

Thanks for your reply.

Best Regards,

Atilla

0 项奖励
回复