iMX6Q Type Differences

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6Q Type Differences

ソリューションへジャンプ
2,120件の閲覧回数
atillametetured
Contributor V

Hello,

Quick question about the three different versions of the application processors iMX6Q.

Is it only the operational temperature that differs between;

1. i.MX 6Dual/6Quad Applications Processors for Industrial Products

2. i.MX 6Dual/6Quad Applications Processors for Consumer Products

3. i.MX 6Dual/6Quad Automotive and Infotainment Applications Processors

If not only the temperature, what else seperates these three?

Best Regards,

Mete

ラベル(2)
1 解決策
2,009件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Atilla

all parts share the same modules, so functionality is identical.

Differencies can be in lifetime, check AN4724,25 i.MX 6  Product Usage Lifetime.

Also automotive parts pass factory tests for compliance with automotive

specifications for use in the harsh automotive environment.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,010件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Atilla

all parts share the same modules, so functionality is identical.

Differencies can be in lifetime, check AN4724,25 i.MX 6  Product Usage Lifetime.

Also automotive parts pass factory tests for compliance with automotive

specifications for use in the harsh automotive environment.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,009件の閲覧回数
atillametetured
Contributor V

Hi Igor,

Thanks for your reply.

Best Regards,

Atilla

0 件の賞賛
返信