iMX6Q Serial Downloader bootmode problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6Q Serial Downloader bootmode problem

3,625 Views
artsiomstaliaro
Contributor IV

Hi,

im using iMX6Q device and set next boot mode - BOOT_MODE[1:0] = 0b01.

I connect USB cable to PC and to OTG1, but no activity on PC (checked by USB View utility).

Im able to connect with JTAG to Cortex-A9 core and step in BootROM.

Please give me right direction, where i should check.

Labels (1)
0 Kudos
Reply
5 Replies

3,124 Views
igorpadykov
NXP Employee
NXP Employee

Hi Artsiom

if you have jtag one can run USB Device SDK test

(imitate iROM in some manner)

i.MX 6Series Platform SDK

Also please check Chapter 8 Avoiding Board Bring-up Problems

Chapter 2 Design Checklist

IMX6DQ6SDLHDG IMX6DQ6SDLHDG, Hardware Development Guide

Also it may be recommended to test with other computers, preferably with Windows XP.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,124 Views
artsiomstaliaro
Contributor IV

Hello, thank you for advice.

I checked with JTAG - PLLs are not started!

How BootROM should configure it? (Maybe exist dependence from Config pins?)

0 Kudos
Reply

3,124 Views
igorpadykov
NXP Employee
NXP Employee

It is interesting.

However is something work at all ?

For example, had you luck to run with jtag small code

from SDK and toggle fore example GPIO ?

I attached very small test (based on SDK) one can try it.

Best regards

chip

0 Kudos
Reply

3,124 Views
artsiomstaliaro
Contributor IV

Yes, i can start code in RAM (0x0090 0000). My little software relase Ethernet PHY from reset by GPIO.

ARM core is working, but only at 24MHz

0 Kudos
Reply

3,124 Views
igorpadykov
NXP Employee
NXP Employee

I think you can check with oscilloscope

signals on NVCC_PLL_OUT,

VDD_ARM_CAP LDO and other LDOs.

Best regards

chip

0 Kudos
Reply