iMX6DL LPDDR2 Routing Rules

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX6DL LPDDR2 Routing Rules

3,914 次查看
tom_perman
Contributor III

Hi,

We are working on a design which uses the iMX6DL with LPDDR2 memory. The Hardware Development Guide (IMX6DQ6SDLHDG) rev 4 gives DDR routing rules in section 3.5. However these appear to be for DDR3. Are there LPDDR2 specific rules?

Thanks,

Tom

标签 (1)
0 项奖励
回复
5 回复数

3,874 次查看
tom_perman
Contributor III

Hi,

Thank you for all your help so far - the information provided has been useful.

I have a final question regarding the length matching. Are there package lengths available for the iMX6DL? This is so that length matching can incorporate both delays due to the PCB and internally within the iMX6DL package. This information has been provided for more modern iMX processors e.g the iMX8MM for matching the LPDDR4 interface. 

Thanks,

Tom 

0 项奖励
回复

3,846 次查看
Yuri
NXP Employee
NXP Employee

@tom_perman 
Hello,

  I've sent You some comments.

Regards,
Yuri.

0 项奖励
回复

3,895 次查看
tom_perman
Contributor III

Hi Yuri,

Thanks for your comments. Is there a reference design available which uses the iMX6DL with LPDDR2? The majority of designs I have come across use DDR3. 

Thanks,

 

Tom 

3,886 次查看
Yuri
NXP Employee
NXP Employee

@tom_perman 
Hello,

  I used request  #00331684 to forward some files. Hope it helps.

Regards,
Yuri.

3,907 次查看
Yuri
NXP Employee
NXP Employee

@tom_perman 
Hello,

  I've sent You some comments directly.

Regards,
Yuri.