Boot from QSPI-NOR flash without SDcard on IMX7

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Boot from QSPI-NOR flash without SDcard on IMX7

跳至解决方案
1,411 次查看
JAEWON
Contributor I

i'm using a i.MX7Dual SABRE and I want to boot use QSPI-NOR flash. 

but for my personal reasons, I can't use the SD card.

I changed the resistance setting by referring to the post below and tried to write without SD card using mfgtool, but it did not work as expected. Is this impossible at all or am I not trying to do it right?

 

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Write-program-to-the-QSPI-NOR-on-i-MX-7D...

标签 (1)
0 项奖励
回复
1 解答
1,401 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using the MCIMX7SABRE  board from NXP? If yes,  you need to follow it.

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,402 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using the MCIMX7SABRE  board from NXP? If yes,  you need to follow it.

 

0 项奖励
回复
1,400 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version BSP are you using?

0 项奖励
回复
1,378 次查看
JAEWON
Contributor I

Sorry for my belated reply. 

I couldn't care because of the holidays and other tasks.The BSP version I'm currently using is 5.4.70_2.3.0, and it seems to be a problem with the board from what the company found out.
Because it is not a regular board, but a little customized board.

 

Thanks for your answer.

0 项奖励
回复