iMX6DL LPDDR2 Routing Rules

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6DL LPDDR2 Routing Rules

3,786件の閲覧回数
tom_perman
Contributor III

Hi,

We are working on a design which uses the iMX6DL with LPDDR2 memory. The Hardware Development Guide (IMX6DQ6SDLHDG) rev 4 gives DDR routing rules in section 3.5. However these appear to be for DDR3. Are there LPDDR2 specific rules?

Thanks,

Tom

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

3,746件の閲覧回数
tom_perman
Contributor III

Hi,

Thank you for all your help so far - the information provided has been useful.

I have a final question regarding the length matching. Are there package lengths available for the iMX6DL? This is so that length matching can incorporate both delays due to the PCB and internally within the iMX6DL package. This information has been provided for more modern iMX processors e.g the iMX8MM for matching the LPDDR4 interface. 

Thanks,

Tom 

0 件の賞賛
返信

3,718件の閲覧回数
Yuri
NXP Employee
NXP Employee

@tom_perman 
Hello,

  I've sent You some comments.

Regards,
Yuri.

0 件の賞賛
返信

3,767件の閲覧回数
tom_perman
Contributor III

Hi Yuri,

Thanks for your comments. Is there a reference design available which uses the iMX6DL with LPDDR2? The majority of designs I have come across use DDR3. 

Thanks,

 

Tom 

3,758件の閲覧回数
Yuri
NXP Employee
NXP Employee

@tom_perman 
Hello,

  I used request  #00331684 to forward some files. Hope it helps.

Regards,
Yuri.

3,779件の閲覧回数
Yuri
NXP Employee
NXP Employee

@tom_perman 
Hello,

  I've sent You some comments directly.

Regards,
Yuri.