iMX6DL LPDDR2 Register Programming Aid

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6DL LPDDR2 Register Programming Aid

ソリューションへジャンプ
2,519件の閲覧回数
tom_perman
Contributor III

Can I confirm that the latest available version of iMX6DL register programming aid is v1.3 (linked below)? There was a reference to a version 1.4 in the comments of the linked page

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX6DL-LPDDR2-Register-Programming-Aid/...

ラベル(1)
0 件の賞賛
返信
1 解決策
2,508件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi tom_perman

 

yes latest version of iMX6DL register programming aid is v1.3.

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,501件の閲覧回数
tom_perman
Contributor III

Thanks for confirming. 

@TheAdmiral  stated the following error with v1.3 in the linked post: 
"Just found an error in the spreadsheet in the calculation of the nWR value of MR1. Will correct this and add a Pre-Charge all command to the MR programming sequence"

Can you give me more details of this error? Are there any other issues with v1.3 I should be aware of?

Thanks,

 

Tom 

0 件の賞賛
返信
2,509件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi tom_perman

 

yes latest version of iMX6DL register programming aid is v1.3.

 

Best regards
igor

0 件の賞賛
返信