iMX6 secure boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 secure boot

2,798 Views
basavaraju_hars
Contributor I

Dear NXP community,

 

I have a Apalis board with an imx6 processor and I am trying to enable a secure boot to this board.

Prerequisite to this, CONFIG_SECURE_BOOT configuration is enabled at configs/apalis_imx6_defconfig.

If this I am trying to give a MAKE and ended in the following error.

Error: arch/arm/imx-common/built-in.o: In finction 'is_hab_enabled' :

u-boot-toradex/arch/arm/imx-common/hab.c:267: undefined reference to 'fuse_read'

Please refer to attachment for more details.

If a give a MAKE with enabling the CONFIG_SECURE_BOOT configuration, build is complete with binary outputs.

Please help us to break this issue.

Thanks in advance.

Labels (1)
0 Kudos
Reply
1 Reply

2,675 Views
joanxie
NXP TechSupport
NXP TechSupport

you can check your bsp hab.c, this is nxp bsp source code:

hab.c\mach-imx\arm\arch - uboot-imx - i.MX U-Boot 

you can try to command bitbake uboot-imx, if you already set CONFIG_SECURE_BOOT configuration,

you also can refer to the AN, chapter 3.4.Configureand buildU-boot to support secureboot,

https://www.nxp.com/docs/en/application-note/AN4581.pdf 

0 Kudos
Reply