iMX6 reference schematic (SPF-27417-C5) and noticed that the two MSB of the address lines were mapped to No Connects on the micron RAM chip

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 reference schematic (SPF-27417-C5) and noticed that the two MSB of the address lines were mapped to No Connects on the micron RAM chip

2,492件の閲覧回数
davidriness
Contributor I

hello -

I was looking at the reference schematic (SPF-27417-C5) and noticed that the two MSB of the address lines were mapped to No Connects on the micron RAM chip.

What was the reason behind this? To load them?

Do the address lines need to be connected?

ラベル(1)
0 件の賞賛
返信
1 返信

2,313件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi David

reason is ability to soder memories with higher densities, where these

signals are present.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信