iMX6 reference schematic (SPF-27417-C5) and noticed that the two MSB of the address lines were mapped to No Connects on the micron RAM chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 reference schematic (SPF-27417-C5) and noticed that the two MSB of the address lines were mapped to No Connects on the micron RAM chip

2,491 Views
davidriness
Contributor I

hello -

I was looking at the reference schematic (SPF-27417-C5) and noticed that the two MSB of the address lines were mapped to No Connects on the micron RAM chip.

What was the reason behind this? To load them?

Do the address lines need to be connected?

Labels (1)
0 Kudos
Reply
1 Reply

2,312 Views
igorpadykov
NXP Employee
NXP Employee

Hi David

reason is ability to soder memories with higher densities, where these

signals are present.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply